Knowledge Base

Generac Power Zone Pro (Sync) via Ethernet

This topic is the install guide for the after-market gateway (part# G0097460) with the universal harness (part# A0006648426) when utilizing the Generac Power Zone Pro® and Power Zone Pro Sync via an Ethernet connection.

Generac Power Zone Pro

image-20250114-182141.png
Power Zone Pro Display Panel
image-20250116-143829.png
Connect to Power Zone Gateway for programming and Modbus TCP connection.

Generac Power Zone Pro Sync

image-20250115-145001.png
image-20250116-152824.png
Display COMPUTER port can be used for programming and Modbus TCP connection.
image-20250116-152959.png
Base controller Ethernet ports can be used for programming.

Modbus Communication Settings and Notes

To confirm port settings, follow the guidelines listed in this section. Settings should correspond to the values provided in the table.

IP:  192.168.3.2

Subnet: 255.255.255.0

DNS:             Leave Blank

Gateway: 192.168.3.100

For firmware version 1.21.9 and prior:

  1. Navigate to Setup>Communications>Modbus Pass Thru.

  2. Modbus TCP Enable and Ignore Unit ID toggles should both be checked.

  3. Confirm that the IP settings correspond to the values in the table.

For firmware version 1.22.1 or newer:

  1. Navigate to Setup>Communications>External Interfaces> Ethernet Built In>Configure>Modbus Gateway >Configure.

  2. Modbus TCP Enable and Ignore Unit ID toggles should both be checked.

  3. Confirm that the IP settings correspond to the values in the table.

If the above two are not applicable:

  1. Navigate to Setup>Communications>Ethernet/Wi-Fi/Bluetooth> Ethernet Icon.

  2. Confirm Ethernet Enabled toggle is on.

  3. Select Static Connection mode, and confirm Static IP address settings as above
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
+

DC+

Red

B+

-

DC-

Black

B-

ETH1

Modbus TCP

*CAT5 cable

‘COMPUTER’ /
Ethernet Port

Harness Relay #1

COM

Blue

2-Wire Start

N/O

White / Blue

*included in harness accessory kit.

Gateway Connection Ports

image4-20250114-183802.png
Gateway Right Panel—GPS antenna and harness I/O connections
image3-20250114-183853.png
Gateway Left Panel—Cellular antenna, power, serial communication ports, and SIM card slot
image-20250116-154106.png
Front panel—ETH1 to be used for Modbus TCP connection.

Check out our knowledge base and support center for information on any technical questions.