Knowledge Base

Power Zone Pro Sync RS485

Configuration for the Power Zone Pro Sync RS485 can be done using the touch screen display. These same screens can also be accessed with a laptop.

The information provided in this section reflects firmware 1.23.2 or newer.

  1. Select Setup menu option at bottom of display.

setup-menu-pzps.jpg
Setup Menu
  1. Enter password for admin access.

Further information will be provided on the generator hardware for a licensed technician.

  1. Expand the Communications module then External Interfaces.

External-Interfaces-full.jpg
RS485 Built In Configuration
  1. Click Configure for the RS485 Built In module.

RS485-BuiltIn.jpg
RS485 Built In Port Details
  1. Enter or update to the following settings:

  • Mode: Modbus Gateway 

  • Baud Rate: 9600 

  • Parity:  None 

  • Stop Bit: 1 

  • Unit ID: 1 

RS485-Config.jpg
RS485 Configuration
  1. Click Apply Changes if entering modifications.

  2. Port Status and Serial Port Configuration will reflect any new settings.

RS485-Port-Stat.jpg
Port Status