Knowledge Base

Gateway Network Diagrams - BMS and Annunciator

This section describes how to use an Advanced Gateway in parallel with a building management system (BMS) and/or remote annunciator. The Advanced Gateway uses Modbus to connect to most generator controllers. Typically, the gateway will connect using the RS-232 or RS-485 serial port that is may also need to be used by BMS and/or remote annunciators. Topics listed in this section provide connection schematics for using these devices together.

Supported Hardware

A full listing of topics is available by expanding the left navigation. On mobile devices, the expand icon may appear at the bottom of the window.