Knowledge Base

Site Deployment Wizard

The Site Deployment Wizard guides field technicians through the steps to activate and configure monitored equipment within the Generac Link platform. Instructions on how to connect the Generac Link Gateway to the monitored equipment can be found in the Controller Wiring Guides.

Configuring and Deploying the Site

Be sure to have your hardware specification sheet available. This wizard requires entry of rated power, amperage, voltage, and other commonly-referenced parameters.

Site Deployment access is required to run this wizard. Access must be toggled on for the user via User Permissions in the Settings menu.

Choose the Site Deployment menu option from the Settings drop-down menu.

Site-Depl-Menu.png
Site Deployment Menu Option

Commissioning the Gateway

The steps in this section provide instructions for commissioning the gateway in order to enable 24x7 connectivity.

For models listed in the table here, the Gateway is attached at the factory before delivery to your site. For such units, the gateway serial number—required to step forward through the Wizard—will be visible through plexiglass. To locate the serial number in earlier models, refer to the packaging with the gateway hardware.

Because the print is small, obtaining the gateway serial number may require snapping a photo and then zooming in order to read all the digits.

Excludes Diesel engines below 200 kW, gas engines G9.0L, 150kW and below, as well as ROW and OEM units.

Using the Wizard, the user is presented with the following screen when registering equipment. When a Gateway serial (not generator) number is entered, the system checks against our database for validation. If the serial number is already in use on the instance, the next button will not be enabled and you will not be able to proceed.

GW-Prompt-Rev.png
Prompt for Gateway Serial Number

After entering a valid Gateway Serial number, the Next button is enabled. Then the user can proceed with completing the Wizard.

Site Name and Equipment

In Step 1 of the installation wizard, the field technician will create a generator equipment profile, describing the physical premise and associated hardware. Some fields have been pre-populated with entries for convenience. If necessary to replace these values, simply type into the field to update from defaults.

  1. Enter a Site Name, describing the location of the equipment. When choosing a name, ensure the entry is unique against other Site Names on the same instance.

  2. For Stationary Sites:

    1. Enter the street address.

    2. A second address line field is optional. This is provided to accommodate a unit or room number.

    3. Type or use the drop down to select the state.

    4. Enter the Zip code. You will be asked to verify this in a modal, which will structure the address according to U.S. Postal Service formatting.

Pg1-Col1.png
Wizard Step 1, Column
  1. For Mobile sites, ensure the radio button is toggled to “Mobile”, the address fields are optional as the unit location will be determined by the GPS on the Generac Link Gateway.

    1. image-20260217-160611.png


  2. Select the Timezone of the equipment using the drop-down menu. This will be reflected in reporting data downstream.

  3. Fields for Building Name, Floor Name, and Room Name are available. Defaults are displayed in this capture. Simply type into the field to replace the defaults.

All fields are required aside from the second address line.

In the second column of the asset profile page, add the remaining details.

  1. Enter a descriptive generator name to facilitate easy reference for maintenance and monitoring.

  2. Enter the manufacturer.

  3. The Controller field is selectable using the drop-down menu. Information on which Controlle Profile to select can be found in the wiring guide.

  4. Model and serial numbers are found with the original equipment packaging.

  5. Enter rated power (in kW) and amperage by typing into the respective fields. These should correspond with the generator’s specification sheet and will populate in the NFPA and other reports.

pg1-col2.jpg
Wizard Step 1, Column 2
  1. Use the radio toggles to select the Output Voltage Type.

  2. Enter the output voltage listed with the hardware specifications. Common presets are available once clicking into the field.

  3. Complete the fuel type entry using the pop-up menu when clicking into the box. 

  4. For gateways that are not attached to the asset at the factory, the serial number is located on the front of the device, and/or included with the product materials.

image-20240418-182221.png
Gateway Serial Number from Packaging
  1. Once the Site and equipment details are complete, the Next button will be enabled.

The wizard provides the user with the option to accept the USPS formatting standard, which includes a Zip Code extension. Latitude and Longitude will populate the location automatically once a street address is accepted by the platform.

Address-Detail.png
Address Verification Modal

In Step 2 of the Installation Wizard, be sure to click the Save & Download button to enable communications with the Advanced Gateway.

box555-save.png
Step 2 Verification: Save and Download

A secondary modal will prompt the user for confirmation. A validation screen appears next, confirming location details as configured by the installer. Sufficient signal strength will be indicated with at least two bars.

Click the Back button if you need to make changes to the entries.

secondary-modal-sd.png

Click Details button to look further at connectivity data. Click Done in Step 3 to return to the Map View.

site-verified.png
Verification Screen

Numerous supporting topics are available in our community knowledge base. Check for equipment-specific support or announcements on future enhancements in our release notes. Full details at https://support.energyservices.generac.com.

Site Modifications

Once a Site is created on the platform, limited modifications are available through the Site and Equipment menu. Administrators can update the site name, Address, time zones, and alarm settings, and telemetry types that populate the live stream (see next section).

image-20260217-160827.png


Once this wizard is complete and saved, generator specifications entered in step 1 of the wizard are not changeable without a Support ticket.

Monitoring

To view generator's live data, click the site pin from the Map View. Be sure to check out our section on trending and telemetry.