Knowledge Base

Viewing Equipment in Real Time

To get to a list of equipment, click a site pin on the Map View landing page, or switch to List View utilizing icon in top-right corner of the screen and select a site from there. At any point, clicking the top banner icons will bring you back to the map.

image-20260217-161620.png

Site Summary

If the site is configured to monitor multiple pieces of equipment, you'll see a summary of all equipment at that location along with any active alarms. Live data streams automatically for up to 15 minutes. When the stream times out, a message will appear — just click it to restart.

The data shown in the table is fully configurable through the Site and Equipment configuration wizard.

image-20260406-210621.png

Drilling Into Equipment

To dig into a specific piece of equipment, click its Details link from equipment card in bottom right corner of site summary or click its row in the data table. If there are active alarms, clicking an alarm record will take you directly to that equipment's Alarm tab.

From the equipment page, you can review telemetry, reports, and alarms to help diagnose potential issues or specific events of interest.

From the equipment you can view telemetry, reports, and alarms to assist with diagnosis of any anomalies.

image-20260217-161838.png

Like the Site Summary, live data here will also stream automatically for 15 minutes and can be restarted the same way if it times out.