Skip to main content
Skip table of contents

Generac Evolution Controller (V3)

This topic is the install guide for the after-market gateway (part# A0009887841) with harness (part# A0009887770, A0009887771, A0009887772) utilizing the Generac Evolution (Air or Liquid Cooled) control panel via Modbus.

NOTE: Please reach out to Generac generator support team or Generac Link support team at least a week in advance with generator serial number. Generac must confirm if the Evolution controller on the generator is capable of supporting advacned data. Please do not proceed onsite without confirmation.

image-20250115-180405.png

Panel Display for the Generac Evolution Control

image-20250115-170336.png

Close View of Port Connections

DTECH9000.png

The GL899 does not have an RS232 port, and requires a RS232 to RS485 converter (DTech DT9000 included in A0009887771 accessories kit). An additional breakout board is required to jump Mobile Link wire harness comm wires to RS232 link side of converter.

Communication Settings and Notes

Settings should correspond to the values provided in this table.

Address:  157

Data Bit: 8

Baud Rate: 115200

Stop Bit: 1

Parity: None

Please refer to Generator installation/ control manuals available on Genservice for information about how to view/ edit communication settings. If Modbus configuration on the controller are different than what is mentioned above, please change the configurations on the Evolution controller to match above.

Note that Evolution controller does not support faster polling. The polling rate will be every 1 second

Equipment Connection Details

Generac Gateway Side Terminations

Description

Harness Wire Color

Equipment Side Terminations

S232 DB9 breakout*

DTECH
DT-9000 RS485 port

2

DC+

A0009887772 Red

Battery +

1

DC-

A0009887772 Black

Battery -

8

Data +

A0009887770 Orange / White

388 (Connector J6—Pin#7)

3-TXD

T/R+

9

Data -

A0009887770 White / Orange

387 (Connector J6—Pin#8)

2-RXD

T/R-

10

Data GND

A0009887770 Blue/ White

Connect to Pin 4 of J6 connector. Note that there is no labelled wire for this pin. The harness wire needs to be inserted and secured on the pin using a tweezer tool by installer

5-GND

GND

Harness Relay #1

COM

A0009887772 Blue

Remote Start—178

N/O

A0009887772 White / Blue

Remote Start—183

Additional breakout board is required to breakout board cover to protect connections and secure to service port.

The DSE899 does not have an RS232 port, hence we need to use a DTECH DT-9000 RS232 to RS485 converter.

* DB9 breakout board needs to be procured separately by installer.

Gateway Connection Ports

image-20251126-201727.png

Pin

Connector

Description

1

A

Plant Supply –ve

2

Plant Supply +ve

3

Digital Output A

4

Digital Output B

5

Flexible Sender Common

6

Flexible Sender A

7

Flexible Sender B

1

B

 

RS485 A

2

RS485 B

3

RS485 Screen

4

CAN H

5

CAN L

6

CAN Screen

Check out our knowledge base and support center for information on any technical questions.

JavaScript errors detected

Please note, these errors can depend on your browser setup.

If this problem persists, please contact our support.