Skip to main content

Power Zone Pro Sync Setup

This section describes a typical setup for the Gateway connecting to the Pro Sync Display RS485 port. A typical setup for the Gateway connection to the RS485 Annunciator is provided in the first illustration.

RS485-Standard.jpg

Typical RS485 Setup

A BMS connection to the Pro Sync display can be achieved with Modbus TCP/SNMP protocol, requiring a BMS-computer connection.

BMS-Ethernet.jpg

BMS Connection Via Modbus TCP/SNMP Protocol

A BMS connection to the RS485 can be achieved with Modbus RTU protocol.

BMS-ModbusRTU.jpg

Gateway Connection with Modbus RTU Protocol

Steps to configure the TCP port are provided in this section.

  1. Via the touch screen display menu: a) Navigate to the Setup menu at bottom of screen b) Navigate to the Communications module c) Select External Interfaces menu option.

image-20240605-125505.png

Communications Module

  1. In the Ethernet Built In module, click the Configure button.

image-20240605-125534.png

Ethernet Built In Module

  1. Click Configure button in the Modbus Gateway module.

image-20240605-125708.png

Modbus Gateway Module

  1. Confirm that Enable and Ignore Unit ID toggles are selected.

  2. To update IP address: a) Navigate to Setup. b) Navigate to Communications c) Use the Ethernet/Wifi/Bluetooth menu option.

image-20240605-130036.png

Updating IP Address

  1. Click the local network icon to view IP address settings.

image-20240605-130606.png

IP Address Settings

  1. Update to the values provided here and be sure to click Apply Changes button.

Ethernet Enabled

Toggled on

Connection mode toggle

Set to Static

IPV4 address

192.168.3.101

Subnet

255.255.255.0

Gateway

192.168.3.100

JavaScript errors detected

Please note, these errors can depend on your browser setup.

If this problem persists, please contact our support.