Connecting Advanced Gateway to PSTS or TX Transfer Switch
The gateway also has the ability to monitor and control an Automated Transfer Switch (ATS) using Modbus protocol.
The schematics is this topic offer further detail for connecting the gateway to a PSTS or TX transfer switch.
PSTS ATC300
The following schematic illustrates the setup for connecting the PSTS–ATC300 controller if there is an existing RS485 connection to either a Power Zone Pro Sync Display or a Deepsea G8601.

PSTS-ATC300-J10
*Once wired, the gateway requires configuration to monitor the transfer switch as well. Configuring the gateway accordingly may require the GES solutions engineering team. To get started we recommend opening a Support ticket.
The following schematic illustrates the setup for connecting the PSTS–ATC900 controller if there is an existing RS485 connection to either a Power Zone Pro Sync Display or a Deepsea G8601.

PSTS-ATC900-J12
The following schematic illustrates the setup for connecting the TX–TXC100 controller if there is an existing RS485 connection to either a Power Zone Pro Sync Display or a Deepsea G8601.

TXC-100-J13