Knowledge Base

User Notification Preferences

Once confirmed via the email invite to the user, every user has the option to update their profile name as well as notification preferences. Both email and SMS alarm notifications are supported.

  1. To access user preferences, click the Settings cog icon in the upper right-hand corner of the browser page of the application, then select Preferences.

Pref-Menu.png
Access to Notification Preferences
  1. In the Preferences modal, a user is setup with a first and last name, email address, and mobile number for notifications. If providing multiple entries, these must be separated by semicolons, as indicated in the modal.

  2. Notifications may be toggled on/off for active alarms or when an alarm is cleared.

  3. Users can also access the Preferences modal later in order to make modifications or additions.

Preferences-modal.png
User Preferences: Standard User View

An administrator can also make updates to these fields after selecting a user at the top of the User Preferences modal.

prefs-select-user.png
User Preferences: Administrator View