Skip to main content
Skip table of contents

Generac Evolution Controller

This topic is the install guide for the after-market gateway (part# G0097460) with the universal harness (part# A0006648426) utilizing the Generac Evolution (Air or Liquid Cooled) control panel via Modbus.

NOTE: Please reach out to Generac generator support team or Generac Link support team at least a week in advance with generator serial number. Generac must confirm if the Evolution controller on the generator is capable of supporting Modbus. Please do not proceed onsite for Modbus wiring without confirmation.

image-20250115-180405.png

Panel Display for the Generac Evolution Control

image-20250115-170336.png

Close View of Port Connections

Modbus Communication Settings and Notes

Settings should correspond to the values provided in this table.

Address:  157

Data Bit: 8

Baud Rate: 115200

Stop Bit: 1

Parity: None

Please refer to Generator installation/ control manuals available on Genservice for information about how to view/ edit communication settings. If Modbus configuration on the controller are different than what is mentioned above, please change the configurations on the Evolution controller to match above.

Note that Evolution controller does not support faster polling. The polling rate will be every 1 second

Equipment Connection Details

Generac Gateway Side Terminations

Description

Harness Wire Color

Equipment Side Terminations

+

DC+

Red

Battery +

-

DC-

Black

Battery -

TX1

Data Transmit

Orange / White

388 (Connector J6—Pin#7)

RX1

Data Receive

White / Orange

387 (Connector J6—Pin#8)

GND

Data GND

Green/ White

Connect to Pin 4 of J6 connector. Note that there is no labelled wire for this pin. The harness wire needs to be inserted and secured on the pin using a tweezer tool by installer

Harness Relay #1

COM

Blue

Remote Start—178

N/O

White / Blue

Remote Start—183

Gateway Connection Ports

image4-20250114-183802.png

Gateway Right Panel—GPS antenna and harness I/O connections

image3-20250114-183853.png

Gateway Left Panel—Cellular antenna, power, serial communication ports, and SIM card slot

Check out our knowledge base and support center for information on any technical questions.

JavaScript errors detected

Please note, these errors can depend on your browser setup.

If this problem persists, please contact our support.