Skip to main content

ComAp InteliGen NT Using GenConfig

These configuration steps require being connected to the controller while running ComAp GenConfig software. Settings should be updated only after initial firmware and configuration updates are complete.

  1. While connected to the controller, choose the Setpoint tab at the top of the window, then choose Comms settings under the Groups heading.

image-20240705-204153.png

GenConfig Setpoints

  1. Update the settings to the entries provided in this step:

  • Contr. Address: 1

  • RS232(1) mode: MODBUS-DIRECT

  • RS232(1)MBCSpd: 9600

  • RS485(1) conv.: DISABLED

  1. Be sure all Access Groups are set to: 0 On.

  2. Click Write to Controller icon to apply changes.

image-20240705-205033.png

Apply Changes

JavaScript errors detected

Please note, these errors can depend on your browser setup.

If this problem persists, please contact our support.